I experience problems to connect the MSP430 target with the MSP-FET430UIF JTAG adapter. The most frequent error message is:
Error: MSP430: Error initializing emulator: Unable to load C:\Program Files (x86)\Texas Instruments\ccsv4\DebugServer\drivers\msp430.dll because The specified module could not be found.
Other errors are:
Error: MSP430: Error initializing emulator: No USB FET was found
Error: MSP430: Trouble Reading Memory Block at 0x13d2 on Page 0 of Length 0xb: Could not communicate with FET
The error can be solved by terminating CCS, power cycle the FET and restart CCS. This is very annoying when I need to restart CCS for each debug session.
CCS version is 4.2.4.00033
OS version Windows7(64-bit)
Is CCS incompatible with the 64-bit version of Windows7? How can the problems be fixed?
Helge