I have an issue with getting the spectrum digital XDS510 emulator working with the LM3S2965 eval board within CCS4.1.3. I have followed all the directions at the following link:
http://processors.wiki.ti.com/index.php/How_to_setup_CCSv4_with_SD_XDS510_for_TI_Stellaris_M3
It seems to progress well...and then receive the following error message within CCS4 output window:
CORTEX_M3_0 : This Target Does Not Support The GEL_DriverString() Function
A pop up also occurs with:
Error connecting to the target:
Error 0x800000240/-141
Fatel Error during: Initialization, OCS,
Error generated by SD scan controller module
Any help or guidance is greatly appreciated.
Best Regards,
John