Hello
I have just installed CCS V5 (Version: 5.1.0.09000)
When I import a project "existing CCS/CCE Eclipse projects" from either CCE V3 or CCSV4 the project imports, the files are displayed in windows explorer when I look at the directory, but they do not display in the CCSV5 project explorer window.
If I create a new blank project it does correctly display in the project explorer window.
Doesn't seem to matter if I check the "Copy projects into workspace" checkbox or not during the import
Also the CVS options don't display under import