Tool/software:
When using the XDS110 debugger for code flashing, the JTAG IR and DR scan paths are unable to circulate the bits in the following configurations:
- Normal JTAG configuration
- 4-pin cJTAG configuration
- 2-pin cJTAG configuration in advanced mode
The same error is reflected across all configurations. Later, even when connected using the serial number, the same error persists. I also used the LaunchPadXL (F280049C) as a standalone debugger, and the same error replicated. And even tried to removing pull-up and pull-down resistors from mcu(F280049C) custom board and tried to flash the code, same error replicated.
I am sharing a screenshot related to the error with this query. I am stumped. What should I do now to resolve the error? Kindly provide me with a solution.
Thanks,
Bhuvana.