I am trying to boot the C674 in a TMDXEVM8148 evaluation board. I can succesfully boot it using CCS and GEL files but what I am trying to achieve is to generate the files necessary (.c, .h, .obj) to include in an external build to create the out file (basically using the compiler/linker externally). I think there are some basic xdctools files that CCS generates with the basic boot information, but I don't know which ones to use. Any help?