Other Parts Discussed in Thread: CCSTUDIO
Hello,everyone
Recently,when I used DM6437 on CCSv5,I find a problem about gel file.
In the path of C:\CCStudio_v3.3\boards\evmdm6437_v2\gel, the evmdm6437.gel version is 1.03
And in the path of C:\ti\ccsv5\ccs_base\emulation\boards\evmdm6437\gel, the evmdm6437.gel version is 1.50.
When I load a application .out file,I find some unexpected erros. If I used evmdm6437.gel (1.03), when I loaded the program,it can not find the entry of main and I can not click the run button ,it seems that it runs freely. However when I used evmdm6437.gel (1.50),it can load and run correctly.
I don’t know why. Could you help me about this,and tell me about the existing problems. thanks.
Regards.
Junqing Zhao