Good day,
I want to determine the code size of my program in the flash memory of EK-LM4F232 in code composer v5.
Where can I get this information.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good day,
I want to determine the code size of my program in the flash memory of EK-LM4F232 in code composer v5.
Where can I get this information.
Thanks,
Hi,
You can find the static memory usage by inspecting the linker map file that is automatically generated inside the output directory (Debug or Release).
From the project explorer, you can open the output directory and search for a file with extension .map. Among other info, it will show the device's memory regions and their usage.
Hope this helps,
Rafael
Do you know which sections are counted toward the 16kB code size limit for the free version of CCS?
desouza said:You can find the static memory usage by inspecting the linker map file that is automatically generated inside the output directory (Debug or Release).
Could CCS translate to decimal values in next release? (other tools do it)
Or at least summarize main values in decimal.
CCSv6 (currently in Beta) has a view called 'Memory Allocation" view that summarizes the memory usage, and shows it in decimal values. This short video gives an overview.
The .out file contains information which is not loaded into the flash memory of the target. e.g. the .out file can also contain symbolic debug information and therefore the size of the .out file isn't an indication of the flash usage.sreelakshmi pemmaka said:my .out file is of 326kb and actual flash is of 256kb
The .map file shows the program uses 0x6cd6 bytes out of the total of 0x40000 bytes of flash, which means only approx 11% of the flash size is used.
Hello All,
I am facing a similar issue of memory maping and havent gone through it much.
Kindly support me with below query
I am having below detail which I got it from .map file.
SRAM (RWX) : origin = 0x20000000, length = 0x0008000
But my data memory is exiding 0x8000 so I am unable to flash the program.
I have checked in memory allocation tab, SRAM memory I can use till 32kb.
Can any one help me out to solve this issue??
Thanks in advance.
Mitesh
If the bitmaps don't need to change at run time, then if bitmaps are declared as const the bitmaps should be placed in flash by the compiler / linker thus reducing the SRAM usage.Mitesh Sirodaria said:I am using a code for interfacing graphical LCD and while interfacing I have given bitmaps value in header file. which is getting compiled.
How are the bitmaps defined in the header file?
This was directed to poster "Mitesh" - as addition to the sound advice advanced by Chester...
Firm/I are not fans of (any) single vendor restricted IDE - thus we avoid CCS. (hard to imagine that ONE vendor - and only ONE vendor - will always (best) satisfy our needs!)
We've enjoyed success w/in the display field - and never would store such image data w/in the (limited) MCU space. External memory - especially fast, modern, 4 bit, serial flash (perhaps even 2 such devices - yielding 8 bits) completely AVOID MCU memory overflow...
Can you show your code, and the increase in SRAM memory usage?Mitesh Sirodaria said:I have added a new header file with bitmaps as const char but it still affects my SRAM Memory. If I don't call those variables(images) in my main function it reduces my memory but as soon as I add it in my main function, SRAM Memory usage gets increased. Although my header file is already added in the project.
Mitesh Sirodaria said:For such small application is it necessary for adding external memory?
Will your applications "always" be so small? If not - what then? (a band-aid solution may not offer long-term comfort)
Image & font data do not belong w/in limited MCU memory space unless the application is extremely high volume - which is unlikely to result for the vast majority - here...
Your move to proper, external memory will insure that a proper solution is delivered now - and long into the future. (when you are surely going to exceed limited capacity, MCU space.) Further - it is likely that w/proper use of external storage - you may chose an MCU w/reduced memory size - reducing your cost...
I opened the .map file and found this :
run origin load origin length init length attrs members
---------- ----------- ---------- ----------- ----- -------
00000000 00000000 00005298 00005298 r-x
00000000 00000000 0000026c 0000026c r-- .intvecs
0000026c 0000026c 00004e14 00004e14 r-x .text
00005080 00005080 0000019a 0000019a r-- .const
00005220 00005220 00000078 00000078 r-- .cinit
20000000 20000000 00000304 00000000 rw-
20000000 20000000 00000200 00000000 rw- .stack
20000200 20000200 000000a0 00000000 rw- .bss
200002a0 200002a0 00000064 00000000 rw- .data
Which of them Will be the Code Size