Other Parts Discussed in Thread: TMS320F2809
Code composer studion 5.2.1, compiler version 6.1, TMS320F2809
I have a structure
typedef struct // 4 MAU
{
UInt32 fSerial : 20;
UInt32 fMonth : 4;
UInt32 fYear : 7;
UInt32 fRes1 : 1;
UInt32 fJobNum : 24;
UInt32 fManu : 7;
UInt32 fRes2 : 1;
} TSerialNum;
and a constant
const TSerialNum cSerialNum =
{
0x54322,
8,
12,
0,
0x4321,
1,
0
};
I would expect a 64-bit value in memory as 0x0100'4321'0C85'4322.
But the " cSerialNum " after compilation is 0x4321'00C8'0005'4322, what is definitely wrong. What's the matter? I can't figure out where the problem is.
Thanks for any help.
Walter