This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS register window EDMA_CC0

Other Parts Discussed in Thread: OMAPL138

Dear E2E:

Is EDMA_CC0 accessible by ARM in OMAPL138?

I use OMAPL138 with emulator "Blackhawk-M".

When emulator is connected to JTAG port and to ARM processor - the EDMA_CC0 is not shown in the "register window" - I can see EDMA_CC1 only.

EDMA_CC0 is shown in "register window" when emulator is connected to the DSP processor on OMAPL138 - I can see both EDMA_CC0 and EDMA_CC1.

That is why I am asking - if ARM processor on OMAPL138 can control EDMA_CC0?

According to data sheet "Memory Map" - EDMA accessible by ARM and DSP processor.

CCS version which I use is: 4.2.4.00033

Thank you fort your help,

Boris Ruvinsky