Other Parts Discussed in Thread: TMS320VC5509A
Team,
I am not sure if it is the proper forum to post my issue. If not, please forward it to the right forum! Thanks!
I am using CCS debug with the Spectrum Digital C5509A DSK. I get the following error when I run the debug:
"
Error connecting to the target:
Error 0x80002280/-1250
Fatal Error during: Target Communication, OCS, Control,
Device driver: Lost USB connection to emulator.
You should ABORT and restart to re-establish the USB link
"
and the CCS Console window also shows, in red:
"
C55xx: Error connecting to the target: Error 0x80002280/-1250 Fatal Error during: Target Communication, OCS, Control, Device driver: Lost USB connection to emulator. You should ABORT and restart to re-establish the USB link.
".
The hardware setup and connection have no problem, because the same set works with another PC.
What should I do to setup my PC so that the debug can find the proper target?
Thanks,
Wendy Fang
TSC, AIP, HPA, TI Dallas