Hello all,
I have an issue: After the guys at Spectrum Digital tested my board (had no issues on their CCS installation) it was returned to me and now I am experiencing the same issues as before - "Error Initializing Emulator". I've seen a few posts regarding this but this issue does not seem to have been resolved in those posts so I figured I'd make a fresh one just in case anyone has recently gotten past this. So in summary, when attempting to run an example on my F28335 EZ-DSP, I receive an error which reads "Error initializing emulator".
1) I am using the onboard emulator.
2) The USB port works fine since I tested my DSK6713 board which initialized and was able to run a program.
3)I've set the target configuration to "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator" connection and chose the "EZDSPF28335" device.
Does anyone know how solve this issue? I don't think I should send the board back since it was verified that it works on "their" system which uses the same CCS version.