This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

adding examples to the ti explorer in ccs 5

Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE

hi

im using ccs 5 and have peripheral explorer kit with tms320f28335 control card along with it.How could you add examples for 28335 in to this .The resource explorer for the installed ccs does not have any examples for 28335.If it can not be added can you provide with some examples?

another doubt if in 'help' to ccs support the 'debug server log' is termed false does that cause any problem?

  • Arun,

    If you install controlSUITE you can point the Resource Explorer in CCS to it and it will allow you to browse the included examples.  It installed in the default location it may discover the examples automatically.

    You can open Resource Explorer from the View menu in CCS.  View -> TI Resource Explorer.  

    If you don't see controlSUITE on the left then you can tell it where it is installed.  Click on the Home button at the top of Resource Explorer.  Then scroll down to the bottom of resource explorer and click the link to configure where packages are located.

    Once it has discovered controlSUITE you can change the packages drop down on the top left to just show controlSUITE content and then expand the tree to the area you are interested in:

    Regards,

    John