Other Parts Discussed in Thread: TMS320F2812, CCSTUDIO
Hi
I am using Code Composer Studio (v3)and the processor TMS320F2812.While i am trying to import an example project i.e PMSM3_3_281X (sprc178 which i got from ti site itself), showing an error like this
pmsm3_3.c] "C:\CCStudio_v3.1\C2000\cgtools\bin\cl2000" -g -q -fr"../obj" -i"./include" -i"../include" -i"../../../../lib/dmclib/cIQmath/include" -i"../../../../lib/drvlib280x/include" -i"../../../../lib/drvlib281x/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/cmd" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_common/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_examples/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_common/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_examples/include" -i"../../DSP281x_headers/include" -d"_DEBUG" -d"LARGE_MODEL" -d"TARGET_IS_F2812" -ml -v28 -@"../build/Debug.lkf" "pmsm3_3.c"
"pmsm3_3.c", line 29: fatal error: could not open source file "DSP281x_Device.h"
1 fatal error detected in the compilation of "pmsm3_3.c".
Compilation terminated.
>> Compilation failure
[DSP281x_DefaultIsr.c] "C:\CCStudio_v3.1\C2000\cgtools\bin\cl2000" -g -q -fr"../obj" -i"./include" -i"../include" -i"../../../../lib/dmclib/cIQmath/include" -i"../../../../lib/drvlib280x/include" -i"../../../../lib/drvlib281x/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/cmd" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_common/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_examples/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_common/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_examples/include" -i"../../DSP281x_headers/include" -d"_DEBUG" -d"LARGE_MODEL" -d"TARGET_IS_F2812" -ml -v28 -@"D:/ragi/ragu/v35x/sys/PMSM3_3_281x/cIQmath/build/Debug.lkf" "DSP281x_DefaultIsr.c"
[DSP281x_PieCtrl.c] "C:\CCStudio_v3.1\C2000\cgtools\bin\cl2000" -g -q -fr"../obj" -i"./include" -i"../include" -i"../../../../lib/dmclib/cIQmath/include" -i"../../../../lib/drvlib280x/include" -i"../../../../lib/drvlib281x/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/cmd" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_common/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_examples/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_common/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_examples/include" -i"../../DSP281x_headers/include" -d"_DEBUG" -d"LARGE_MODEL" -d"TARGET_IS_F2812" -ml -v28 -@"D:/ragi/ragu/v35x/sys/PMSM3_3_281x/cIQmath/build/Debug.lkf" "DSP281x_PieCtrl.c"
[DSP281x_PieVect.c] "C:\CCStudio_v3.1\C2000\cgtools\bin\cl2000" -g -q -fr"../obj" -i"./include" -i"../include" -i"../../../../lib/dmclib/cIQmath/include" -i"../../../../lib/drvlib280x/include" -i"../../../../lib/drvlib281x/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/cmd" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_common/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_examples/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_common/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_examples/include" -i"../../DSP281x_headers/include" -d"_DEBUG" -d"LARGE_MODEL" -d"TARGET_IS_F2812" -ml -v28 -@"D:/ragi/ragu/v35x/sys/PMSM3_3_281x/cIQmath/build/Debug.lkf" "DSP281x_PieVect.c"
[DSP281x_SysCtrl.c] "C:\CCStudio_v3.1\C2000\cgtools\bin\cl2000" -g -q -fr"../obj" -i"./include" -i"../include" -i"../../../../lib/dmclib/cIQmath/include" -i"../../../../lib/drvlib280x/include" -i"../../../../lib/drvlib281x/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/cmd" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_common/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_examples/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_common/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_examples/include" -i"../../DSP281x_headers/include" -d"_DEBUG" -d"LARGE_MODEL" -d"TARGET_IS_F2812" -ml -v28 -@"D:/ragi/ragu/v35x/sys/PMSM3_3_281x/cIQmath/build/Debug.lkf" "DSP281x_SysCtrl.c"
[DSP281x_GlobalVariableDefs.c] "C:\CCStudio_v3.1\C2000\cgtools\bin\cl2000" -g -q -fr"../obj" -i"./include" -i"../include" -i"../../../../lib/dmclib/cIQmath/include" -i"../../../../lib/drvlib280x/include" -i"../../../../lib/drvlib281x/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/cmd" -i"../../../../../../../c28/dsp281x/v100/DSP281x_headers/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_common/include" -i"../../../../../../../c28/dsp281x/v100/DSP281x_examples/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_common/include" -i"../../../../../../../c28/dsp280x/v110/DSP280x_examples/include" -i"../../DSP281x_headers/include" -d"_DEBUG" -d"LARGE_MODEL" -d"TARGET_IS_F2812" -ml -v28 -@"D:/ragi/ragu/v35x/sys/PMSM3_3_281x/cIQmath/build/Debug.lkf" "DSP281x_GlobalVariableDefs.c"
Build Complete,
1 Errors, 0 Warnings, 0 Remarks.
But the file 'DSP281x_Device.h" is already been added in the project.
Could you please suggest ways to rectify this error?
Regards
Ragi