Other Parts Discussed in Thread: HALCOGEN
Dear Experts,
I am using CCS V5.3.0 with TI ARM compiler V5.0.1 on Hercules MCU (TMS570LS3137ZWT).
When trying to apply MISRA-C:2004 checker with [Required] option, I found the following warnings which I could not understand and get rid of...
Please kindly help me here:
1. Warning on rule 10.1 : #1393-D (MISRA-C:2004 10.1/R) The value of an expression of integer type shall not be implicitly converted to a different underlying type if it is not a conversion to a wider integer type of the same signedness
This warning is given on the statement generated by HALCoGen V3.03.01, in the function of "adcGetData();" of source file of "adc.c".
"uint32_t count = adc->GxINTCR[group] >= (uint32_t)256U ? s_adcFiFoSize[index][group] : s_adcFiFoSize[index][group] - (uint32_t)(adc->GxINTCR[group] & 0xFF);"
where "adc" is a structure pointer with type of "adcBASE_t *", GxINTCR[] is an element of the structure with "uint32_t" type.
2. Warning on rule 12.8: #1407-D (MISRA-C:2004 12.8/R) The right-hand operand of a shift operator shall lie between zero and one less than the width in bits of the underlying type of the left-hand operand
This warning is given on the statement generated by HALCoGen V3.03.01, in the function of "adcInit();" of source file of "adc.c".
"adcREG1->BNDCR =(8U << 16U)|(8U + 8U);"
where "adcREG1" is a structure pointer with type of "adcBASE_t *", BNDCR is an element of the structure with "uint32_t" type.
3. Warning on rule 14.1: #1465-D (MISRA-C:2004 14.1/R) There shall be no unreachable code
This warning is given on the following statement:
do{
/* any statement here...*/
}while(0);