I have a reel of MSP430F2112 I bought from Digikey. They are QFN32 parts. CCS V4 is not recognizing the part correctly and thinks it is a 21x1 part.
I have version 4.0.2.01003 of Code Composer Studio (I just upgraded using help->Software Updates since the original installation had the same problem).
I went through the CCS wizard to create an MSP430F2112 project and added __MSP430F2112__ to the pre-defined names, and it gives the error. If I create a separate project for the MSP430F2111 and add __MSP430F2111__ to the predefined names, it allows the code to be uploaded.
I am using the EZ430U Rev 2.0 to program the chip. Is that the problem? Do I need to buy another programmer?
The only code I have loaded so far is a simple main just to watch the debugger work:
#define VAR_DECLS
#include <msp430.h>
void main(void)
{
while(1)
{
// do nothing
}
}
Thanks,
Greg