Hello,
I use a TMS320C28345 and I have a problem with CCS ; in fact, I'm using an 256kB external memory and I'd like to load a program of 250kB in it.
With my techniques, I need to put a table of data in .out build by CCS. For that, I have to resize the memory section (384kB available on SARAM H and 128kB on SARAM L). The program will be load in RAM and then execute to be loaded in external memory.
The problem is that when I put the table in static section (.h), the .ebss and .cinit is filled approximately at the same time and I can't put the whole table, even if I split the sections.
I have also tried to put the table in main.c but the size of local variable memory is not big enough.
Have you any idea to solve this problem ?
Thank you very much for your help.