Hi,
I been working quite well with an EVM6455, on-board emulator and CCSv3.2 as installed from the product CD.
I still haven't to get CCSv4 working satisfactorily on a PC with no other CCS installations.
I can use CCSv4 with the DSK (download, run and debug code) but when I try and talk to the Mezz the debugger appears to get locked up and I can't continue.
If I download to the DSK the debugger runs and stops at main pretty much instantly. When I download to the Mezz usually I don't get to main. Once or twice it has got to main, like with the DSK, but then it locks up when I try and do something else.
SD support suggested a problem with the Mezz or the Mezz connector but how can this be the case when I don't have any problems using CCSv3.2? We haven't had the EVM very long.
Is anyone successfully using both boards, the on-board emulator and CCSv4?
I'm quite willing to believe that I'm doing something wrong but at the moment I can't think what else to try.
Thanks,
Matt