Why is CCS showing the "?" icon, and if the line is hovered over the pop over says "Syntax error". This is in an MSP430 project.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Why is CCS showing the "?" icon, and if the line is hovered over the pop over says "Syntax error". This is in an MSP430 project.
If there are no errors reported by the compiler in the CCS build console, then this Syntax error is likely coming from the Eclipse indexer that comes built-in with CCS. You can take a look at and adjust the indexer settings and even disable the indexer from Project Properties->C/C++ General->Indexer. There is also a way to disable the indexer markers without disabling the indexer itself. If you disable the indexer completely you will lose the capabilities of code completion and navigation to declaration/definition. However, you can disable the indexer marker by going to Window->Preferences->General->Editors->Text Editors->Annotations and uncheck all three checkboxes for "C/C++ Indexer Markers".