Other Parts Discussed in Thread: TM4C123GH6PGE, TM4C129ENCPDT
I am using CCS 6.0.1.00040 with a Tiva TM4C129ENCPDT and TM4C123GH6PGE and have an XDS100v2 Spectrum Digital emulator. After starting a debug session and loading the program on either target I go to Tools --> Hardware Trace Analyzer --> Interrupt Profiling (or any of the other predefined trace analyzers). From there, the Trace Configuration dialog opens and shows the following. The only option for Transport Type in the drop-down list is SWO Trace, which technically isn't possible with the XDS100. Based on the documentation for the Trace Analysis User's Guide, there should be an ETB option in the Transport Type drop-down list, but there isn't. I can manually type in ETB, but that does not appear to work correctly. Is this a bug in CCS v6?