Hello!
I bought a LAUNCHXL-F28377S to program a DC-DC-Converter but it is impossible for me to get an example link, memory map and debug correctly.
When I import an example like "C:\Ti\controlSUITE\development_kits\LAUNCHXL-F28377S\LaunchPadDemo" I get only linker and mapping errors.
The same when I import something like "C:\Ti\controlSUITE\device_support\F2837xS\v200\F2837xS_examples_Cpu1\adc_soc_epwm"
I loaded a project from Github "github.com/.../TMS_Skype_Petcam" and after some changes in the project properties I could load it into the debugger. Then I exchanged the old HEADER-Files in the project with the new ones "C:\Ti\controlSUITE\device_support\F2837xS\v200\F2837xS_headers\include" nothing works. Linker and Mapper errors.
Then I tried it with the TI-Cloud but there are no examples available for the TMS320F28377S.
I have installed: (all should be up to date)
CCS V6.1.3.00034
ControlSuite Examples for F2837xS V2.0
IQMath V1.6
FPUfastRTS V1.0
CLAmath V4.01.00.00
Please can someone give me a working project folder for "C2000 Delfino MCUs F28377S LaunchPad Development Kit" LAUNCHXL-F28377S for TI Cloud or CCS Win10 with included Libs and Headers in the project that I can import and will work.
Best would be if it is a copy of a Project that is following configured.
CPU-Clock 200MHz
Peripheral-Clock 50Mhz
using external 10MHz Quartz
and the LED D9 or D10 is blinking
Thanks a lot for your HELP!!!
Best Regards
Harald