This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS510 USB

Hi

I have a problem using the Spectrum Digital XDS510 USB emulator.

When trying to connect to a target this is what i get:

Error connecting to the target:
Error 0x80000240/-2082
Fatal Error during: Initialization, OCS,
Device driver: Emulation Connection Loss Detected on Target CPU.
It is recommended to RESET EMULATOR.  This will disconnect each
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.


I/O Port = 0

Board Name: F28035 XDS510 Emulator
Cpu Name: TMS320C2800_0

Abort:        Close Code Composer Studio.
Retry:        Try to connect to the target again.
Cancel:        Remain disconnected from the target
Diagnostic:    Run diagnostic utility.

This happens on different EVMs. When using the XDS100 onboard emulator it works fine.

When i run the Reset Emulator. I get this error message:

Failed to reset the emulator: This error was generated by TI's USCIF driver.  SC_ERR_CTL_NO_TRG_POWER <-180> The controller has detected a target power loss. The user must turn-on or connect the power supply for the target. 

The emulator seems to be working according to Windows

I have installed CCS3.3 and the driver+patch downloaded from Spectrum Digitals homepage:

http://support.spectrumdigital.com/ccs33/

The version of CCS is:

 

I have tryed to connect to our "Multi Axis DMC EVM (R3)" board and the "2 ch buck EVM" with the same result.

Hope you can help me out.