Tool/software: Code Composer Studio
Hi,
I am trying to use XDS560 PCI JTag emulator to connect a PCI board (based on TMS320C6412). my CCS version is 3.3 and using Windows 7 x64 SP1, and this is the error I get
Error connecting to the target:
Error 0x80000240/-314
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.
SC_ERR_PGM_FPGA_FAIL_AFTER <-314>
An attempt to program the emulator FPGA failed.
The failure occurred after loading data.
A likely cause is the final FPGA state is bad.
Sequence ID: 0
Error Code: -314
Error Class: 0x80000240
Board Name: C64xx XDS560 Emulator
Cpu Name: CPU_1
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
Thanks
Arash