Tool/software: Code Composer Studio
I am writing a code and want to check if it is MISRA C compliant. I switched on the MISRA C option in Project > Properties > General >Advanced Options > MISRA C. But it has only been added with MISRA C 2004. Is there a way to add an add-in or anything of that kind so as to make it compatible with MISRA C 2012?
And can anyone provide me a method or flowchart of how to go ahead with MISRA C and its documentation so that I write the code in such a way it is compliant and also how to create a compliance matrix?
Any help would be helpful.
Thank you in advance.