This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Decoding of "raw data" field in ofd output

It seems to me that "raw data" should simply be the code or initialized data that is associated with a given symbol/location.  For example, here's a snippet from the generated xml:

- <section>
  <name>.sts</name>
  <physical_addr>0xc04ce2dc</physical_addr>
  <virtual_addr>0xc04ce2dc</virtual_addr>
  <raw_data_size>0x30</raw_data_size>
  <reloc_count>0x0</reloc_count>
  <line_count>0x0</line_count>
  <addr_size>0x1</addr_size>
  <alignment>0x4</alignment>
  <data>true</data>
- <file_offsets>
  <raw_data_ptr>0x5990</raw_data_ptr>
  <reloc_ptr>0x0</reloc_ptr>
  <line_ptr>0x0</line_ptr>
  </file_offsets>
  <raw_data>AAAAAAAAAAAAAAAAAAAAgAAAAAAAAAAAAAAAAAAAAIAAAAAAAAAAAAAAAAAAAACA</raw_data>
  </section>

If I look at that same file in a hex editor, I see the following for the "raw data" section:

However, if I load the out file using CCS and look at the corresponding location I see:

Can someone explain how these all fit together?  Is this a bug or am I completely misunderstanding this field?

Thanks,
Brad