Other Parts Discussed in Thread: LAUNCHXL-CC1350-4, , SYSBIOS
Tool/software: Code Composer Studio
Hello, it's my first question in the forum ...
I want to test a board that complies with the specifications of the TIDA-01228, once all connected to a LAUNCHXL-CC1350-4 Rev-A. I'm in charge of the LCSense1350DK project in my CCS8 ... and I get the following error when running DEBUG:
Description Resource Path Location Type
fatal error: inc/hw_types.h: No such file or directory LCSense1350DK line 46, external location: C:\ti\tirtos_cc13xx_cc26xx_2_21_00_06\products\bios_6_46_01_37\packages\ti\sysbios\family\arm\cc26xx\Timer.c C/C++ Problem
gmake: *** [../src/sysbios/rom_sysbios.am3g] Error 2 LCSense1350DK C/C++ Problem
gmake: *** [build-25636449] Error 2 LCSense1350DK C/C++ Problem
gmake: *** [C:/ti/TIDA01228/LCSense1350DK/src/sysbios/rom_sysbios.aem3] Error 2 LCSense1350DK C/C++ Problem
gmake: Target 'all' not remade because of errors. LCSense1350DK C/C++ Problem
gmake.exe: *** [package/cfg/rfPacketTx_pem3.xdl] Deleting file `package/cfg/rfPacketTx_pem3.c' LCSense1350DK C/C++ Problem
gmake.exe: *** [package/cfg/rfPacketTx_pem3.xdl] Deleting file `package/cfg/rfPacketTx_pem3.h' LCSense1350DK C/C++ Problem
gmake.exe: *** Deleting file `package/cfg/rfPacketTx_pem3.xdl' LCSense1350DK C/C++ Problem
gmake[1]: *** [build-25636449-inproc] Error 1 LCSense1350DK C/C++ Problem
gmake[1]: *** [cc26xx_Boot.o] Error 1 LCSense1350DK C/C++ Problem
gmake[1]: *** [cc26xx_Timer.o] Error 1 LCSense1350DK C/C++ Problem
gmake[1]: *** [rom_sysbios.obj] Error 1 LCSense1350DK C/C++ Problem
gmake[1]: Target 'all' not remade because of errors. LCSense1350DK C/C++ Problem
recipe for target '../src/sysbios/rom_sysbios.am3g' failed makefile.libs /LCSense1350DK/src line 56 C/C++ Problem
recipe for target 'build-25636449-inproc' failed subdir_rules.mk /LCSense1350DK/Debug__TI line 33 C/C++ Problem
recipe for target 'build-25636449' failed subdir_rules.mk /LCSense1350DK/Debug__TI line 30 C/C++ Problem
recipe for target 'cc26xx_Boot.o' failed makefile /LCSense1350DK/Debug__TI line 137 C/C++ Problem
recipe for target 'cc26xx_Timer.o' failed makefile /LCSense1350DK/Debug__TI line 140 C/C++ Problem
xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2: .xdchelp /LCSense1350DK line 209 C/C++ Problem
directory "C:/ti/tirex-content/tirtos_cc13xx_cc26xx_2_21_00_06" on package path does not exist LCSense1350DK C/C++ Problem
Invalid project path: Include path not found (C:\ti\tirex-content\tirtos_cc13xx_cc26xx_2_21_00_06). LCSense1350DK pathentry Path Entry Problem
Product 'SimpleLink CC13x0 SDK' v1.30.0.06 is not currently installed. A compatible version 1.60.0.21 will be used. LCSense1350DK LCSense1350DK Problem
XDCpath repository 'C:/ti/tirex-content/tirtos_cc13xx_cc26xx_2_21_00_06' cannot be found! Visit project's 'Properties > General > RTSC' tab to adjust the XDCpath. LCSense1350DK LCSense1350DK Problem
I have dealt with CCS7, and now with CCS8 ... but always the same problem and I do not find the / inc / directory anywhere.
Thanks.