Tool/software: Code Composer Studio
Hi All,
we’re experiencing some strange CCS installer behavior. After selecting a number of Code Generation Tool updates, Code Composer downloads the tools and stores them at ccsv8\eclipse\downloads, asks for a restart and exits, which is correct so far.
But then nothing happens. In the Windows 7 task manager you can see that the automated update process “ccs_update_8.1.0.00011.exe” has been started, but the corresponding dialog will not open for about 15 minutes. After that it will start with the installation. Unfortunately the installation will not succeed. It will only install one CGT update at a time. All other previously downloaded tools will be removed from the ccsv8\eclipse\downloads folder.
What’s even worse is that Code Composer Studio does already register the presence of the tools right after downloading them. You can verify that in HelpàAbout Code Composer StudioàInstallation Details right before restarting CCS. If the installer fails, registration and presence of the tools are out of sync. You have to manually remove the already registered CGT, that could not be installed and try again and wait for another 15 minutes for the installer to run.
Clearly need a fix for this. Any idea?
Best regards,
Flux.