Other Parts Discussed in Thread: TMS320F2811
I want to work with the TMS320F2811, aber i have a problem with the connection between my Computer : CCSv4 and the Microcontrollerplatform. When I debug, i become the following message :
Error connecting to the target:
Error 0x80000200/-1142
Fatal Error during: OCS,
Processor blocked debug accesses. An operation was attempted while
the CPU was in a non-debuggable context. To continue to honor the debug
context, press Cancel. To force debug access, press Rude Retry.
and in the console appears : DSP281x_Peripheral.gel', line xxx: the function 'GEL_WatchAdd' is not supported.
So i become the folowing two picture:
Has anyone any idea how to resolve this problem?
Thanks,
sg.wissem