Other Parts Discussed in Thread: MSPWARE, CSD, MSP430WARE
Tool/software: Code Composer Studio
Hi, I'm having a hard time trying to alter one of the MSPware GRLIB driver to support the very common SSD1963. with a 480x272 color graphics display. All there is is some old 96 x 96 pixel display example.
Anyhow there is an example of a GRlib with no display driver and I am trying to add the low level routines to make it work. I can't get the program to compile without errors. One that has me baffled is I when I try to call a function from within another function, I get a # 19 error- 'extra text after expected end of number' The basic code is below.
Thanks for any help!
void SetAddress(unsigned int 1X, unsigned int 1Y)
{
WriteCommand(0x2A); //Set Column Address
WriteData((1X));//I get an error here- #19 extra text after expected end of number
...
...
}
void WriteData(uint16_t usData)
{
CSD=0;
PBOUT= usData; //output the 16)
WRD=0; //Write timing
WRD=1;
CSD=1;
}