Hi,
I am trying to link new files to the existing CCSv4.2 project. I have the macros.ini file in the project directory. When I try to link a new source file to the project, the environment uses the absolute path (without letting end user know). The ideal way would be that the environment can first search the macros.ini and see if it applies, or let the user choose the absolute path or a macro.
Without doing this, it is very hard to build a portable project, especially under Clearcase. It is very dangerous that some files could be from a different view than the user thought.
Currently we manually change the .project file every time we need to hand off. However we hope this feature can be added. Thanks.
Best Regards,
Gary