This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS V8.1 for 2812 - Module Ordering in Memory

Part Number: TMS320F2812

Tool/software: Code Composer Studio

Previously, I was importing a legacy project from CCS V3.3 to CCS V8.1. With your help, I was able to get my legacy v3.3 projects to build without errors or warnings in CCs V8.1. The problem I am now chasing is trying to get the linked output to match up with the desired memory locations. I have used the Link Order tab to set my run-time library (rts2800_ml.lib) to be placed first in the linked out put. My desire is to have the boot28.asm.obj from the library to be the first module located in flash memory. However, I am getting other project modules, not in the library, placed ahead of the boot28 module. Also, the first module from the rts library is "fd_mpy28.asm.obj" followed by the boot28.asm.obj. The Link Order tab is set up as detailed below:

-lrts2800_ml.lib

lib/Flash2812_API_V210/lib/Flash2812_API_V210.lib

lib/IQmath/v15a/lib/IQmath.lib

CP_FLASH.cmd

Also, are there other mechanisms within CCS V8.1 to set the order that modules are built in the project? Thanks for your help.

Terry Stifflemire