This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZ430-Chronos problem with limited code size example

Dear all,

I'm an experienced software developer but completely new in programming of micro controllers. I bought a eZ430-Chronos and started making some tests with the CCS limited core edition. I'm using the 868MHz version. I'm able to build a new image and to download it to the watch.

The problem is that there is a difference in functionality between the uncestricted version of the example code and the size limited version. This applies also to the pre-compiled *.txt-files of the sports watch application which are delivered by TI.

E.g. the stopwatch-application and the buzzer don't work in the restricted version. Is this a bug or is it due to the code size limitation? As I wanted to start my own tests based on the stopwatch-application and don't have a CCS-License I can't do anything more now.

Can anybody help me?

Best regards from Germany

Jürgen

Normal 0 21 false false false DE X-NONE X-NONE