Part Number: CCSTUDIO-KEYSTONE
Tool/software: Code Composer Studio
Hi Team,
I am working with C2000 series device with CCS platform.
I recently noticed one issue: While trying to load a program from the debug window ;the program gets flash in to the device.
Now after rebuilding the project without cleaning the project , the .out file that is generated has gets some changes.
With cleaning the same project and building it ; I found the file got some changes. (compared through a file comparator).
There is one more issue with the program building is : the instructions / logic in the program isn't changed , but it happed a couple of time that the program halts / stops working on the same hardware.
When looking for the fault, probing through XDS110 and taking some tests through Debug window- results are good.
I am unable to understand this issue.
Please help me out in leaning how building a project works and the .OUT file is processed + generated every time the build command is executed.
Thanks and Regards,
Jesal Patel