Other Parts Discussed in Thread: MSP430WARE, MSP430G2553
Tool/software: Code Composer Studio
I am attemptingto compile the example
msp430f524x_adc10_11.c
from "dev.ti.com/tirex/#/?link=Software%2FMSP430Ware%2FDevices%2FMSP430F5XX_6XX%2FMSP430F5232%2FPeripheral%20Examples%2FRegister%20Level%2Fmsp430f524x_adc10_11.c"
using a MSP430F5232 selected as a code composer project and the code from msp430f524x_adc10_11.c
Description Resource Path Location Type
gmake: Target 'all' not remade because of errors. msp430f524x_adc10_11 C/C++ Problem
gmake: *** [main.obj] Error 1 msp430f524x_adc10_11 C/C++ Problem
#20 identifier "ADC10SREF_1" is undefined main.c /msp430f524x_adc10_11 line 99 C/C++ Problem
#20 identifier "ADC10SHS_1" is undefined main.c /msp430f524x_adc10_11 line 97 C/C++ Problem
#20 identifier "ADC10RES" is undefined main.c /msp430f524x_adc10_11 line 98 C/C++ Problem
#20 identifier "ADC10ON" is undefined main.c /msp430f524x_adc10_11 line 96 C/C++ Problem
#20 identifier "ADC10MSC" is undefined main.c /msp430f524x_adc10_11 line 96 C/C++ Problem
#20 identifier "ADC10MEM0" is undefined main.c /msp430f524x_adc10_11 line 142 C/C++ Problem
#20 identifier "ADC10MCTL0" is undefined main.c /msp430f524x_adc10_11 line 99 C/C++ Problem
#20 identifier "ADC10IV" is undefined main.c /msp430f524x_adc10_11 line 134 C/C++ Problem
#20 identifier "ADC10INCH_0" is undefined main.c /msp430f524x_adc10_11 line 99 C/C++ Problem
#20 identifier "ADC10IE0" is undefined main.c /msp430f524x_adc10_11 line 113 C/C++ Problem
#20 identifier "ADC10IE" is undefined main.c /msp430f524x_adc10_11 line 113 C/C++ Problem
#20 identifier "ADC10ENC" is undefined main.c /msp430f524x_adc10_11 line 112 C/C++ Problem
#20 identifier "ADC10CTL2" is undefined main.c /msp430f524x_adc10_11 line 98 C/C++ Problem
#20 identifier "ADC10CTL1" is undefined main.c /msp430f524x_adc10_11 line 97 C/C++ Problem
#20 identifier "ADC10CTL0" is undefined main.c /msp430f524x_adc10_11 line 96 C/C++ Problem
#20 identifier "ADC10CONSEQ_2" is undefined main.c /msp430f524x_adc10_11 line 97 C/C++ Problem
#2580-D pragma vector= accepts numeric arguments or "unused_interrupts" but not ADC10_VECTOR main.c /msp430f524x_adc10_11 line 126 C/C++ Problem
these identifiers appear to be correct according to SLAU208Q–June 2008–Revised March 2018 I have atttemped on a machine with code composer 6 and code composer 8 with the same errors