Part Number: PROCESSOR-SDK-AM437X
Tool/software: Code Composer Studio
Hello everyone,
i've an AM437 IDK Board and installed the CCS on a Windows 7 PC.
this is my first time using an Evaluationboard from TI, please be pation with me :)
First at all, i try to follow the Basic exaples (1.1.3.1.) "hello World" example with no operating system (as shown in this:
After creating the project with CCS and making a Test connection to the board the result of the test connection is:
"....
The JTAG DR Intergrity scan-test has succeeded.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]
..."
so, i think the connection is succesfull?
i connected the Board with the deliverd USB Cable.
but if i want to start to debug with the hello world code the CCS gives an error code:
"...
Error connecting to the target:
(Error - 1266 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package. 8.0.903.6)
..."
my question:
- why is the board on reset, how can i un reset it?
- do i need more hardware device between the PC and the Board? like an Debuger board?
Best regards,
I.T.