This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: Error during firmware load after an update with CCS7

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: MSP-EXP432E401Y

Tool/software: Code Composer Studio

Hi, 

      I'm working with CCS7 and two evaluation boards, the MSP-EXP432E401Y and MSP-EXP432P401R. The CCS/ version is 7.4.0.00015 

After an CCS update I always get this error when I try to debug a project:

CORTEX_M4_0: GEL Output: 
Memory Map Initialization Complete
CORTEX_M4_0: File Loader: Failed to initialize flash programming: Unknown property "FlashResetBeforeLoadSetting"
CORTEX_M4_0: GEL: File: C:\WG\Debug\WG.out: Load failed.


what is the problem?

thank you,

Tommaso