The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: armopt.exe experienced a segmentation fault TI Compiler18.12.3

Tool/software: TI C/C++ Compiler

Code-Repository

The Code inside this repository led to a segmentation fault. 

This Code compile under VisualStudio19 and with the GNU v7.2.1 (provided with Code Composer Studio)

This is the .pp file: 1drv.ms/.../s!AqJ2WVYwAYEujN4eKALwMjSX0V-bnA

This is the output: 

**** Build of configuration Debug__TI for project comtest ****

"C:\\ti\\ccs910\\ccs\\utils\\bin\\gmake" -k -j 8 all -O 
 
Building file: "../tm4c1294ncpdt_startup_ccs.c"
Invoking: ARM Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-arm_18.12.3.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O0 --include_path="C:/Users/mathi/workspace_v9/comtest" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-arm_18.12.3.LTS/include" --define=ccs="ccs" --define=PART_TM4C1294NCPDT -g --c11 --c++14 --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="tm4c1294ncpdt_startup_ccs.d_raw"  "../tm4c1294ncpdt_startup_ccs.c"
Finished building: "../tm4c1294ncpdt_startup_ccs.c"
 
Building file: "../main.cpp"
Invoking: ARM Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-arm_18.12.3.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O0 --include_path="C:/Users/mathi/workspace_v9/comtest" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-arm_18.12.3.LTS/include" --define=ccs="ccs" --define=PART_TM4C1294NCPDT -g --c11 --c++14 --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="main.d_raw"  "../main.cpp"
 
>> Compilation failure
subdir_rules.mk:9: recipe for target 'main.obj' failed
"C:/Users/mathi/workspace_v9/comtest/comms/details/message_check.h", line 164: warning #1-D: last line of file ends without a newline
"C:/Users/mathi/workspace_v9/comtest/comms/details/DispatchMsgIdRetrieveHelper.h", line 91: warning #1-D: last line of file ends without a newline
"../main.cpp", line 34: warning #112-D: statement is unreachable
 
INTERNAL ERROR: C:\ti\ccs910\ccs\tools\compiler\ti-cgt-arm_18.12.3.LTS\bin\armopt.exe experienced a segmentation fault
                  while processing function <unknown> file C:\\Users\\mathi\\AppData\\Local\\Temp\\{D04CADB2-C408-4889-B414-F25F34A68380}
 
This is caused by a defect in the TI C/C++ Optimizer.
TI Customer Support may be able to suggest a workaround to avoid this.
 
Upgrading to the newest version of the compiler may fix this problem.
 
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler".  See the link titled
"Submitting an issue".
 
We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment
 
gmake: *** [main.obj] Error 1
Building file: "../Handler.cpp"
Invoking: ARM Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-arm_18.12.3.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O0 --include_path="C:/Users/mathi/workspace_v9/comtest" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-arm_18.12.3.LTS/include" --define=ccs="ccs" --define=PART_TM4C1294NCPDT -g --c11 --c++14 --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="Handler.d_raw"  "../Handler.cpp"
"C:/Users/mathi/workspace_v9/comtest/comms/details/message_check.h", line 164: warning #1-D: last line of file ends without a newline
"C:/Users/mathi/workspace_v9/comtest/comms/details/DispatchMsgIdRetrieveHelper.h", line 91: warning #1-D: last line of file ends without a newline
Finished building: "../Handler.cpp"
 
gmake: Target 'all' not remade because of errors.

**** Build Finished ****