This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: install CCs 3.3 Platinum on XP+ service pack 3, and got error 1334

Part Number: CODECOMPOSER

Tool/software: Code Composer Studio

Hello,

I try to install CCs 3.3 Platinum on XP+ service pack 3.

I got error 1334.

I try to install the CCs3.3 on another computer ( XP) and on virtual machine ( VM ) + XP + service pack 3 on it.

But, in all those cases the message error 1334 is return .

See at: http://processors.wiki.ti.com/index.php/CCStudio_FAQ#Q:_I_get_installation_errors_when_I_try_to_install_CCS_or_install_a_CCS_Service_Release._How_can_I_get_it_to_install_properly.3F

Error 1334": This error occurs occasionally when installing on a Windows machine with the language set for something other than English. The issue doesn't occur for all non-English languages, but just a small handful. A workaround is to set the Windows language to English for the duration of the installation (and switch back when the installation is complete)."

So, I install on VM +XP+SP 3 , the english edition only. But the error message is still return.

Have any one have idea, what is wrong?

 

Regards.

Asher.