Hi,
We have developing a gui using LM3s9B92's graphic library .The GUI is designed mostly using push buttons widgets and development environment is CC4.
Stellaris In-circuit debugger is used for debugging.
In the debugg mode it will start from main and continue ther in the while loop for any widget notification .so we can see home page of gui.
But if we press any widget the debugging will not go to that call back widget function .ie widget functions are not able to debugg.
So could you place tell me any way of debugging widget based application.? Any simulator available for this target.
Advanced thanks
Anoop/k
. ie. while connecting to target using incircuit debugger