Tool/software: Code Composer Studio
Yesterday I was having trouble trying to write to registers of my EVM5517 DSP. Today I seem to have gone significantly backwards.
I think I may have tried a "Run/Load..." command, trying to send my program to the DSP. Now I can only get the following error message when I try to debug:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.1.0.00012)
Is it possible that I may have overwritten the EEPROM while doing my "Load" command? How could I reprogram the EEPROM if that is the case?
Thanks in advance.