Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hi,
I have a problem with connection between sensor and collector. For sensor example (sleepy device) i use CC1310 launchpad (TI15.4 Stack SDK 3.20.00.23) and for collector example i use CC1312R1 lauchpad (TI15.4 Stack SDK 3.20.0.68 & TI15.4 Stack SDK 3.30.00.03). First connection between sensor and collector is successfull. Then I successfully disassociate sensor from collector with pressing button on sensor board. When I pressing button on sensor board for associate (Starting...), the sensor joined successfully (State changed: 3) but the problem occurs with the Config message. On the sensor side constantly displays error "dataCnf: 64" (getting config message) and on the collector side, it never displays "ConfigRsp" and constantly displays "!Responding". With the sniffer help i figured out that the sensor gets config message and sends response message successfully but the collector ignores that message. How can I solve this problem? I want to reconnect the sensor to the collector without reseting any of them.
Thank you for your ansfer.
Regards, Aleš