hi all
does anyone know of a tool similar to the addr2line utility? or found a way to extract that information using one of the CGT utilities?
the addr2line utility converts an address to a line number/file pair, but unfortunately only works with ELF files (and the CGT output COFF).
cheers,
sam
for reference:
nobss@WS3055:~/$ addr2line -h
Usage: addr2line [option(s)] [addr(s)]
Convert addresses into line number/file name pairs.
If no addresses are specified on the command line, they will be read from stdin
The options are:
@<file> Read options from <file>
-b --target=<bfdname> Set the binary file format
-e --exe=<executable> Set the input file name (default is a.out)
-i --inlines Unwind inlined functions
-j --section=<name> Read section-relative offsets instead of addresses
-s --basenames Strip directory names
-f --functions Show function names
-C --demangle[=style] Demangle function names
-h --help Display this information
-v --version Display the program's version
addr2line: supported targets: elf64-x86-64 elf32-i386 a.out-i386-linux pei-i386 pei-x86-64 elf64-l1om elf64-little elf64-big elf32-little elf32-big plugin srec symbolsrec verilog tekhex binary ihex
Report bugs to <http://www.sourceware.org/bugzilla/>