This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F2417: Reset error using dual image in RAM and ROM

Part Number: MSP430F2417

Tool/software: Code Composer Studio

Hi,

I have used ram memory for bootloader image and flash memory for application firmware. The application firmware creates a copy of the flash image into an external EEPROM and switches into bootloader firmware.

Then the bootloader firmware copies the image from EEPROM to internal flash and runs the application. I am getting a 0xffe reset vector error while jumping into the application from bootloader firmware.

Even I couldn't overwrite the reset vector address of the application from the bootloader.Bootloader reset vector address 0x110A

Application Reset vector address 0xFFFE (default).

I have attached both liker files. Kindly help me with how to handle the reset vector using the dual images in RAM and ROM.

SECTIONS
{
.bss : {} > RAM /* Global & static vars */
.data : {} > RAM /* Global & static vars */
.TI.noinit : {} > RAM /* For #pragma noinit */
.sysmem : {} > RAM /* Dynamic memory allocation area */
.stack : {} > RAM (HIGH) /* Software system stack */

#ifndef __LARGE_CODE_MODEL__
.text : {} > RAM /* Code */
#else
.text : {} >> RAM /* Code */
#endif
.text:_isr : {} > RAM /* ISR Code space */
.cinit : {} > RAM /* Initialization tables */
#ifndef __LARGE_DATA_MODEL__
.const : {} > RAM /* Constant data */
#else
.const : {} >> RAM /* Constant data */
#endif
//.bslsignature : {} > BSLSIGNATURE /* BSL Signature */
.cio : {} > RAM /* C I/O Buffer */

.pinit : {} > RAM /* C++ Constructor tables */
.binit : {} > RAM /* Boot-time Initialization tables */
.init_array : {} > RAM /* C++ Constructor tables */
.mspabi.exidx : {} > RAM /* C++ Constructor tables */
.mspabi.extab : {} > RAM /* C++ Constructor tables */
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
#ifndef __LARGE_CODE_MODEL__
.TI.ramfunc : {} load=RAM, run=RAM, table(BINIT)
#else
.TI.ramfunc : {} load=RAM | FLASH2, run=RAM, table(BINIT)
#endif
#endif
#endif

.infoA : {} > INFOA /* MSP430 INFO FLASH Memory segments */
.infoB : {} > INFOB
.infoC : {} > INFOC
.infoD : {} > INFOD

/* MSP430 Interrupt vectors */

.reset : {} > RESET /* MSP430 Reset vector */
}

/**************************   Application Linker

MEMORY
{
SFR : origin = 0x0000, length = 0x0010
PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
RAM : origin = 0x2100, length = 0x1000 //modified
INFOA : origin = 0x10C0, length = 0x0040
INFOB : origin = 0x1080, length = 0x0040
INFOC : origin = 0x1040, length = 0x0040
INFOD : origin = 0x1000, length = 0x0040
FLASH : origin = 0x3100, length = 0xCEBE
FLASH2 : origin = 0x10000,length = 0xA000
BSLSIGNATURE : origin = 0xFFBE, length = 0x0002, fill = 0xFFFF
INT00 : origin = 0xFFC0, length = 0x0002
INT01 : origin = 0xFFC2, length = 0x0002
INT02 : origin = 0xFFC4, length = 0x0002
INT03 : origin = 0xFFC6, length = 0x0002
INT04 : origin = 0xFFC8, length = 0x0002
INT05 : origin = 0xFFCA, length = 0x0002
INT06 : origin = 0xFFCC, length = 0x0002
INT07 : origin = 0xFFCE, length = 0x0002
INT08 : origin = 0xFFD0, length = 0x0002
INT09 : origin = 0xFFD2, length = 0x0002
INT10 : origin = 0xFFD4, length = 0x0002
INT11 : origin = 0xFFD6, length = 0x0002
INT12 : origin = 0xFFD8, length = 0x0002
INT13 : origin = 0xFFDA, length = 0x0002
INT14 : origin = 0xFFDC, length = 0x0002
INT15 : origin = 0xFFDE, length = 0x0002
INT16 : origin = 0xFFE0, length = 0x0002
INT17 : origin = 0xFFE2, length = 0x0002
INT18 : origin = 0xFFE4, length = 0x0002
INT19 : origin = 0xFFE6, length = 0x0002
INT20 : origin = 0xFFE8, length = 0x0002
INT21 : origin = 0xFFEA, length = 0x0002
INT22 : origin = 0xFFEC, length = 0x0002
INT23 : origin = 0xFFEE, length = 0x0002
INT24 : origin = 0xFFF0, length = 0x0002
INT25 : origin = 0xFFF2, length = 0x0002
INT26 : origin = 0xFFF4, length = 0x0002
INT27 : origin = 0xFFF6, length = 0x0002
INT28 : origin = 0xFFF8, length = 0x0002
INT29 : origin = 0xFFFA, length = 0x0002
INT30 : origin = 0xFFFC, length = 0x0002
RESET : origin = 0xFFFE, length = 0x0002
}

/****************************************************************************/
/* Specify the sections allocation into memory */
/****************************************************************************/

SECTIONS
{
.bss : {} > RAM /* Global & static vars */
.data : {} > RAM /* Global & static vars */
.TI.noinit : {} > RAM /* For #pragma noinit */
.sysmem : {} > RAM /* Dynamic memory allocation area */
.stack : {} > RAM (HIGH) /* Software system stack */

#ifndef __LARGE_CODE_MODEL__
.text : {} > FLASH /* Code */
#else
.text : {} >> FLASH2 | FLASH /* Code */
#endif
.text:_isr : {} > FLASH /* ISR Code space */
.cinit : {} > FLASH /* Initialization tables */
#ifndef __LARGE_DATA_MODEL__
.const : {} > FLASH /* Constant data */
#else
.const : {} >> FLASH | FLASH2 /* Constant data */
#endif
.bslsignature : {} > BSLSIGNATURE /* BSL Signature */
.cio : {} > RAM /* C I/O Buffer */

.pinit : {} > FLASH /* C++ Constructor tables */
.binit : {} > FLASH /* Boot-time Initialization tables */
.init_array : {} > FLASH /* C++ Constructor tables */
.mspabi.exidx : {} > FLASH /* C++ Constructor tables */
.mspabi.extab : {} > FLASH /* C++ Constructor tables */
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
#ifndef __LARGE_CODE_MODEL__
.TI.ramfunc : {} load=FLASH, run=RAM, table(BINIT)
#else
.TI.ramfunc : {} load=FLASH | FLASH2, run=RAM, table(BINIT)
#endif
#endif
#endif

.infoA : {} > INFOA /* MSP430 INFO FLASH Memory segments */
.infoB : {} > INFOB
.infoC : {} > INFOC
.infoD : {} > INFOD

/* MSP430 Interrupt vectors */
RESERVED0 : { * ( .int00 ) } > INT00 type = VECT_INIT
RESERVED1 : { * ( .int01 ) } > INT01 type = VECT_INIT
RESERVED2 : { * ( .int02 ) } > INT02 type = VECT_INIT
RESERVED3 : { * ( .int03 ) } > INT03 type = VECT_INIT
RESERVED4 : { * ( .int04 ) } > INT04 type = VECT_INIT
RESERVED5 : { * ( .int05 ) } > INT05 type = VECT_INIT
RESERVED6 : { * ( .int06 ) } > INT06 type = VECT_INIT
RESERVED7 : { * ( .int07 ) } > INT07 type = VECT_INIT
RESERVED8 : { * ( .int08 ) } > INT08 type = VECT_INIT
RESERVED9 : { * ( .int09 ) } > INT09 type = VECT_INIT
RESERVED10 : { * ( .int10 ) } > INT10 type = VECT_INIT
RESERVED11 : { * ( .int11 ) } > INT11 type = VECT_INIT
RESERVED12 : { * ( .int12 ) } > INT12 type = VECT_INIT
RESERVED13 : { * ( .int13 ) } > INT13 type = VECT_INIT
RESERVED14 : { * ( .int14 ) } > INT14 type = VECT_INIT
RESERVED15 : { * ( .int15 ) } > INT15 type = VECT_INIT
USCIAB1TX : { * ( .int16 ) } > INT16 type = VECT_INIT
USCIAB1RX : { * ( .int17 ) } > INT17 type = VECT_INIT
PORT1 : { * ( .int18 ) } > INT18 type = VECT_INIT
PORT2 : { * ( .int19 ) } > INT19 type = VECT_INIT
RESERVED20 : { * ( .int20 ) } > INT20 type = VECT_INIT
ADC12 : { * ( .int21 ) } > INT21 type = VECT_INIT
USCIAB0TX : { * ( .int22 ) } > INT22 type = VECT_INIT
USCIAB0RX : { * ( .int23 ) } > INT23 type = VECT_INIT
TIMERA1 : { * ( .int24 ) } > INT24 type = VECT_INIT
TIMERA0 : { * ( .int25 ) } > INT25 type = VECT_INIT
WDT : { * ( .int26 ) } > INT26 type = VECT_INIT
COMPARATORA : { * ( .int27 ) } > INT27 type = VECT_INIT
TIMERB1 : { * ( .int28 ) } > INT28 type = VECT_INIT
TIMERB0 : { * ( .int29 ) } > INT29 type = VECT_INIT
NMI : { * ( .int30 ) } > INT30 type = VECT_INIT
.reset : {} > RESET /* MSP430 Reset vector */
}

/****************************************************************************/
/* Include peripherals memory map */
/****************************************************************************/

-l msp430f2417.cmd

Thanks,

Param.