Other Parts Discussed in Thread: TMS320F28379D, , AMC1200, C2000WARE
Tool/software: Code Composer Studio
Dear TI ,
I am Duc from South Korea. I am sorry for my English, Hope you guy understand.
I am trying to use the Delta- sigmal filter module (SDFM) in LaunchPad TMS320F28379D to get the ADC value from AMC1303M2520 -> But it not work :(
1) I am following the code in the control suite - Device support TMS320F28379D
\v210\F2837xD_examples_Cpu1\sdfm_filters_sync_cpu
2) TMS320F28379D launchpad
I connect to AMC1303M2520 To "J2-pin 18 - GPIO123 SD1_C1(1)(CLOCK) "
and "J2-pin 17 -GPIO122 SD1_D1(1) (DATA) "
3) CONFIG IN the "sdfm_filters_sync_cpu" TI example code
pinMuxoption = SDFM_PIN_MUX_OPTION3; // DUC TEST
Because it confige for pin 122 ->137
4) After connecting the correct wiring of AMC1303M2520
AMC1303M2520 ±250 mV 22 kΩ Uncoded CMOS - 20Mhz
+ I insert the input with 50mv sinusoidal waveform (waveform generator)
+ By checking the output of AMC1303M2520 I can see the CLK and DATA signal
HOWEVER, The Filter1_Result in the CCS 8.0 alway show 4096 whatever I do ????
5) I really dont know what is the problem in my configuration? , if you guy have a simple example for 28379D launchpad. Please share with me.
6) Finally, in terms of Isolated Current or Voltage sensor, Could you tell me which is more stable and has a long-distance ?, Sigma-Delta modulator (like AMC1303) or Differential Output voltage (like AMC1200) ?
Thank you so much