This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP-FET: MSP-FET : can't resolve "No USB FET was found" error with CCS studio

Part Number: MSP-FET
Other Parts Discussed in Thread: MSP430F6638, , MSP430WARE

Tool/software: Code Composer Studio

Hello,

I am using MSP430F6638 mcu and I am trying to run some code with CCSstudio. The problem is that when I am trying to debug the program the MSP-FET can't be found : MSP430: Error initializing emulator: No USB FET was found. I am using the 4-Wire JTAG Communication and I am powering the MCU from an external supply so I made the J1 connection :

I also checked the power supply and I do have the right voltage. So I don't if there is  some drivers or some tools that I should install or check if they are installed but I really don't know why the FET isn't found. Here is below my JTAG connections : Since C1 should not exceed 2.2 nF I used a 2 nF cap. I am using v9 of CCSstudio. 

Can someone help please ?

Thank you,

Best regards,

Mike