Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
My customer is facing the same issue of the original thread.
According to the thread, there are two workarounds:
a) Disable secure boot in Windows10
b) Update the Blackhawk Emulation package
Customer cannot take a) due to security reason, so b) is the only option.
One problem is their PC is not connected to network, so CCS on-line update feature cannot be used.
The CCS version is v8.3.
Question:
Is it possible just update the Blackhawk emulation package without updating CCS itself?
If so how?
Below thread mentioned how to extract the Blackhawk driver from CCS offline package.
https://e2e.ti.com/support/tools/ccs/f/81/t/709012
But as far as I looked at CCS9.3.0.00012_win64 off-line installer,
there is no such directory “featurerepo/binary” nor package “com.bh.ccstudio.emulation.win32_root_<version number>”
Thanks and regards,
Koichiro Tashiro