This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2642R: How can I change the default On-Chip Flash Setting for CortexM3/M4?

Part Number: CC2642R

Tool/software: Code Composer Studio

Hi,

Is it possible to change the default "On-Chip Flash" for CortexM3/M4 for a DSS script environment?

I know I can do it for a workspace from CCS via the GUI, but is there a way to change the default for the DSS scripting environment?
I'm working on the CC2642 device and I'm having trouble with the default setting of "Necessary Sectors Only (Return untouched content within sector)".
I'd like to change it to "Necessary Sectors Only" as that works for me.

Is there a file which contains these default settings?  Even If I had to hack those files, I'd like to do that if possible.

Judah