Tool/software: Code Composer Studio
With CCS 9.3.0 under Ubuntu 18.04.4 LTS the Stack Usage view wasn't displaying the Inclusive Size column. E.g.:
If set SWT_GTK3=0 prior to starting CCS, which is the work-around for CCS IDE flickers on mouse movement when ROV and ReX is opened on Linux, then the Inclusive Size is displayed:
Is it worth updating the description of EXT_EP-9563 or the [FAQ] Certain views like the Getting Started view, App Center, Resource Explorer, and Code Analysis views are blank in CCS Linux. How do I fix this? to mention that the Stack Usage view is also affected?