This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6414: Using old compiler with CCSv6

Part Number: TMS320C6414

Tool/software: Code Composer Studio

I’d like to use the old code composer compiler/linker version 4.36, from inside the new code composer studio 6.x.  I’m able to load different versions of compiler using a link that you sent me earlier, but it did not list versions this old.  Is there a way to trick the CCS 6.x environment to use the compiler/linker files from this 4.36 version?  I.E. Is there a setup or configuration file that I could edit from one of the newer compiler versions that would allow me to point to this old compiler?