Part Number: TMS320F280049C
Tool/software: Code Composer Studio
In the past, I have been able to debug interrupts in my code by simply inserting breakpoints so that the code is "paused" when the interrupt is triggered.
I have done this in multiple example files with no issues. I am now working on a much larger code that was written long before I started working on it. The reason I mention this is because I am not sure if any of the settings have been altered from the defaults of the example files.
I inserted a pair of interrupts that should be triggered by the HLC in a CLB block (as per several of the CLB example files). The code builds with no errors, but when I try to debug the interrupts using breakpoints while the code is running on the platform, I get this response:
When I try to enable the breakpoint, I get an error message in a dialog box saying that no code is associated with line 612 in my file. Can someone explain to me what is going on and what I can do to resolve this issue?