Other Parts Discussed in Thread: UNIFLASH
QUESTION 2 after implementing solution 1) :::
We Implemented Solution 1 provided below in CCS5.5 , the new processor RM44 is showing in the processor selection , but the Debug does not show flash setting .
QUESTION 2) Is there any solution for RM44 flash setting to be showing in Debug menu of CCS 5.5
Tool/software: Code Composer Studio
QUESTION 1) :::
Due to the Project Requirements we want to Keep Using to CCS version 5.5 . We do not want to upgrade to later version of CCS .
CCS version 5.5 does not display RM44L920 procession in the Processor Variant Selection
Is there any Method or Process or Script to add the RM44L920 to the CCS 5.5
SOLUTION TO QUESTION 1)
Hello Chandre,
CCS 5.5 doesn't support some new devices such RM44Lx, and TMS570LS07x etc. You needs to copy the cmd file, and xml file from new CCS folder to CCS55 folder.
1. the linker cmd files are located in ccs_base\arm folder
2. flash related files are in ccs_base\hercules folder
3. gel files are in ccs_base\emulation\gel folder
If those files don't solve your problem, please check with CCS team at:
Code Composer Studio™ forum
Thanks and Regards,
QJ Wang